Need spec for ENET_REF_CLK and PCI_E clock(CLK1_P/N) in MX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Need spec for ENET_REF_CLK and PCI_E clock(CLK1_P/N) in MX6Q

913 Views
jim_lin
NXP Employee
NXP Employee

Hello,

can't find the detailed requirement for the follow two clock: 1. ENET_REF_CLK, 2. PCI_E clock supplied from CLK1_P/CLK1_N.

Need the following information for reference:

OSC/125MHz for ENET_REF_CLK (#V22) : VIH VILTolerance High time Low timeRise time Falling time Jitter

PCIE/100MHz for CLK1_P/N (#C7,#D7) : Duty cycleToleranceRise time Falling time JitterVoltage swing



The information is required to choose the right components when composing the schematics.


Thank you,

Jim.

Labels (1)
Tags (2)
0 Kudos
1 Reply

477 Views
Yuri
NXP Employee
NXP Employee

Please use the Hardware Development Guide for i.MX6.

< http://cache.freescale.com/files/32bit/doc/user_guide/IMX6DQ6SDLHDG.pdf >

According to section 2.7 (Oscillator tolerance) it is recommended using the official (RMII, PCIe)

specifications. We can refer to Table 2-20 (24 MHz crystal tolerance

guidelines)  of the Development Guide, assuming stability (thermal, voltage and

other) of PLL output clock is fully defined by external crystal / oscillator,

and i.MX6  meets USB, PCIe, Ethernet clock specs.

  Also, please refer to i.MX6 RMII timing specs in corresponding Datasheets.

0 Kudos