AnsweredAssumed Answered

CAN transmission can not be completed after starting one transmission

Question asked by Kun Xu on Oct 31, 2013
Latest reply on Nov 1, 2013 by Kun Xu


Hi , I started one transmission of MSCAN using the code as follows. However, the program is always running in the code"while ( (CAN1TFLG & txbuffer) != txbuffer);". And can not jump out. I checked the registers, and the CAN1TFLG=0b00000110. Which means TX0 buffer in not empty after I start one transmission. What is the problem?

___________________________________________________________________________

......

CAN1TBSEL = CAN1TFLG; /* Select lowest empty buffer */

txbuffer = CAN1TBSEL; /* Backup selected buffer */

......

CAN1TFLG = txbuffer; /* Start transmission */

while ( (CAN1TFLG & txbuffer) != txbuffer); /* Wait for Transmission* completion*/

_________________________________________________________________________

Outcomes