Is there a manual that describes in detail what are all the possible BSPCFG_xxxxx_xxx definitions that can be used in user_config.h for for the K60?
I’ve searched everywhere to no avail.
Thanks,
Mark
Hi Mark,
Short answer. No.
Longer answer. The board header file contains all the definitions that can be overridden in the user_config.h. Example file for the TWR-K70F120M is the twrk70f120m.h header in the BSP.
If you are using CW10.x and MQX4.0.x the user_config.h header is associated with a XML file that can display the summary of all the BSPCFG_xxxx_xxx definitions as shown below.
The MQX Development team try to balance the most features and capabilities with each BSP/RTOS port they provide.
Regards,
David
For some reason this forum doesn't like the text so here is a PrtScr shot of it on notepad. ???