Hi
I downloaded L3.0.35_4.0.0_ER_SOURCE from http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=i.MX6D&nodeId=018rH3ZrDRB24A&fpsp=1&t... this link.
When I tried untar the file using tar -zxvf ,I got a folder named L3.0.35_4.0.0_ER_SOURCE and inside it there was a folder pkg.
Inside that I again untar the folder linux-3.0.35.tar.bz2 and I got a folder named linux-3.0.35.
But I wants to know how PMIC MMPF0100 handles power mangement and on/off features.
For that I searched for the folder /rpm/BUILD/linux-3.0.35/drivers/mxc/pmic/ .
But I didnt see such files.
Could anyone tell me how to get these files.
Regards
Divya R Dharan
should be 'drivers/regulator/pfuze100-regulator.c'
Robby
You can see the source code directly from the git repo:
http://git.freescale.com/git/cgit.cgi/imx/linux-2.6-imx.git/log/?h=imx_3.0.35_4.0.0
If you want to do it through LTIB, install it, and run this
./ltib -m prep -p kernel; cd rpm/BUILD/linux
Leo
Dear Leonardo
When I have given ./ltib -m prep -p kernel ,It entered in LTIB configuration menu.
Could you please tell which configuration I have to select?
Regards
Divya R Dharan
If it is the first time you run ltib, you will end up in that menu. So, just enter to the menu, save and quit. Source should be on rpm/BUILD/ linux (this is in fact a soft link which points to linux-XXXX, whe the kernel resides).
Leo