AnsweredAssumed Answered

How to Add Micron 29f32g08cbaca to imx25 core board

Question asked by guru guru on Oct 20, 2013
Latest reply on Nov 19, 2013 by Lily Zhang
Branched to a new discussion

Dear All,

 

I have changed the samsung nand flash with Micron (29f32g08cbaca Nand flash which has 224 bytes spare size) on imx25 core board.

 

Now i have booting up the board through sd card (my u boot.bin in sd card only ). it is saying that in the boot message "No Nand device found !!" when i booted up with Micron.

 

Please any one provide me the input to work with Micron 29f32g08cbaca on imx25 core booard.

 

And How i can load the u boot .bin file to Micron 29f32g08cbaca through free scale advanced tool kit. i tried but nothing happened.

 

what are changes should i need to do with u boot and kernel 2.6.31?

 

i need to boot the board In NAND flash boot swith mode with Micron

 

Note: Now i am booting the board through sd card .

 

Regards,

Guru

.

Outcomes