AnsweredAssumed Answered

K60 flash programming problem

Question asked by Jeffrey Berezin on Oct 18, 2013
Latest reply on Oct 23, 2013 by Hui_Ma

I have created a processor expert project in Codewarrior 10.4 for Kinetis TWR-K60D100M with MK60DN512VLQ10 processor.  I can run the project fine in flash when debugging, but when I try to flash the same file using the lightening bolt icon I get the following error where it thinks the image size is zero bytes.  Any help would be appreciated here.  I checked the elf file on disk and it is about 11K.

fl::target -lc "RFID_FLASH_OSJTAG"
fl::target -b 0x20000000 0x10000
fl::target -v off -l off
cmdwin::fl::device -d "FTFL_PFlash512" -o "128Kx32x1" -a 0x0 0x7ffff
cmdwin::fl::image -f "C:\\Users\\jberezin\\workspace\\RFID\\FLASH\\RFID.elf" -t "Auto Detect" -re on -r 0x0 0x7ffff -oe off
cmdwin::fl::erase image
 Beginning Operation ...    
------------------------- 
Auto-detection is successful.   
  File is of type Elf Format.   

Image size is 0 bytes, nothing to erase.   
Nothing to erase.  No sectors selected 
Performing target initialization ...    
Erase Command Succeeded.   
cmdwin::fl::write
------------------------- 
Using restricted address range 0x00000000 to 0x0007FFFF   
Programming file C:\Users\jberezin\workspace\RFID\FLASH\RFID.elf   
Auto-detection is successful.   
  File is of type Elf Format.   

 0 Bytes Programmed, Check Restricted Address Range   
Program Command Succeeded   
fl::target -lc "LC for Simple Flash"
fl::target -b 0x20000000 0x10000
fl::target -v off -l off
cmdwin::fl::device -d "FTFL_PFlash512" -o "128Kx32x1" -a 0x0 0x7ffff
cmdwin::fl::image -f "C:\\Users\\jberezin\\workspace\\RFID\\FLASH\\RFID.elf" -t "Auto Detect" -re on -r 0x0 0x7ffff -oe off
cmdwin::fl::erase image
 Beginning Operation ...    
------------------------- 
Auto-detection is successful.   
  File is of type Elf Format.   

Image size is 0 bytes, nothing to erase.   
Nothing to erase.  No sectors selected 
Performing target initialization ...    
Erase Command Succeeded.   
cmdwin::fl::write
------------------------- 
Using restricted address range 0x00000000 to 0x0007FFFF   
Programming file C:\Users\jberezin\workspace\RFID\FLASH\RFID.elf   
Auto-detection is successful.   
  File is of type Elf Format.   

 0 Bytes Programmed, Check Restricted Address Range   
Program Command Succeeded   

Outcomes