AnsweredAssumed Answered

iMX Yocto: Adding ffmpeg & mongoose to iMX6 image

Question asked by Tejas Shah on Oct 17, 2013
Latest reply on Oct 23, 2013 by Leonardo Sandoval Gonzalez

Hello,

 

I am trying to create an image using yocto for iMX6 sololite board and want to include ffmpeg & mongoose in my image.

I added ffmpeg & mongoose in conf/local.conf by using IMAGE_INSTALL_append but while it is running, it keeps on

giving me an error that:

 

ERROR: Nothing PROVIDES 'ffmpeg'

ERROR: Nothing PROVIDES 'mongoose'

 

I need help in getting these two packages in my final image.

 

I have installed gst-ffmpeg in my image. Is it possible to use gst-ffmpeg in place of ffmpeg to segment a .mp4 file into .ts file segments (HLS segments)?

I looked up on google to find examples related to using gst-ffmpeg, but I wasn't successful.

 

It is very urgent.

Outcomes