Hi
I am using codewarrior 10.3 in windows my task is to develope touchpad with 12 electrodes.
Im using the processor MK40DX256VLQ10
Each electrode is connected to channel TSI0_ch0, TSI0_ch5....TSI0_ch15...
the problem is when i write a value to threshold_0 register it accepts
but then i write value to other register except Threshold_0 reg it creates hard fault..
its urgent
please help...
regards
shabana
CW10.3 is an old verison, could you please update to CW10.5? It can be downloaded from:
Hi,
I have also tried CW10.5 and used the latest TSS library(TSS 3.1.0).. still the problem is not solved.