AnsweredAssumed Answered

Vybrid MCC in Linux without having M4 running

Question asked by Johannes Traxler on Oct 4, 2013
Latest reply on Oct 21, 2013 by Johannes Traxler

Hello,

 

I have a program running in linux userspace which initializes MCC (mcc_initialize). The M4 core is not running, i.e. no image was loaded.

Additionally I create two endpoints. I experience that the program crashes after this operations!

 

Is this because there is no application running on M4?

Or can this error have any other reasons?

 

Currently I do not have the appropriate M4 application ready and as a starting point I just want to initialize the MCC and its endpoints from linux side. Data transfer will not be done!

 

Thanks,

Johannes

Outcomes