I am having trouble running 2 different versions of freescale software and keeping the jungo drivers working. I need to run cw_hc12_v5.1_special and cw_mcu_v10.1_se.
the 10.1 installs and runs perfect. v5.1 will install but it fails to load and run the jungo driver. it fails even if i am logged in as administrator, right click and "run as administrator",
virus scan is disabled, and it is removed from the domain.
I am running windows 7 enterprise.
Richard, try installing CW5.1 not into Program Files folder.
Rick,
Program Files in Win >=7 is special folder. When application installed in one of PF subfolderss tries to write some settings also to PF folder, windows redirects writing and reading of such data files to App Data \ Roaming folder. Some programs see this on-the-fly redirection well, and some not. CW5.1 seems having problems with this Win7 feature. So just install to c:\CW, or c:\Freescale\CW or whatever you may like, but not in to Program Files.
I recommend to install it into
c:\freescale\cw_5.1
Installing development tools into 'program files' will put it onto Windows special control which can have bad side effects.
Richard,
is this problem solved?
on our side both of these two versions are installed on my computer. they are running well and no driver problem happens.
We couldn't see your screenshot, please upload it again
please upload the error screenshot?
in device manger, the jungo driver appears normal?