Hello,
I'm doing a master final project using MPC5643L and CodeWarrior for MPC55xx, MPC56xx 2.8.
One of the objectives of the project is to download code via serial communications (UART/CAN) while the program is running just with changes made from the version that is running. It would appreciate any ideas for doing this.
Thanks,
Aratz
Hi Aratz,
Make your query little clear.
Does you are expecting to run your code at u-boot ??
Regards,
Sarath
Hello,
I'm using a program that compiles from languages used in standard IEC 61131-3 to C.
So the idea is to have any application running on the platform and when I make a change in the program that uses 61131-3 standard, just send information regarding this program via CAN/UART.
Regards,
Aratz