AnsweredAssumed Answered

i.MX6S SDXC support

Question asked by Paul_Kang Employee on Sep 29, 2013
Latest reply on Oct 4, 2013 by SergioSolis

Hello,

 

According to our i.MX6S RM, it says i.MX6S can support SDXC as like below.

 

Up to 832 Mbps of data transfer for SDXC cards using 4 parallel data lines in SDR(Single Data Rate) mode

 

But, I wonder if our BSP can support SDXC as well and there is no problem to support over 1TB capacity as well. According to SDXC spec, it seems to support up to 2TByte but I am not sure if our BSP or file system can have limiation to do it.

 

Best regards,

Paul

Outcomes