AnsweredAssumed Answered

KINETIS KL25 USB CDC and SERIAL

Question asked by DolomitiLynx on Sep 27, 2013
Latest reply on Sep 28, 2013 by Erich Styger

I have designed  a KL25 microcontroller based board, and I'm now in the testing and validation phase of the development process. I would like to let the board  be recognizable from a PC as a serial port. This would give me the possibility to test  the USB (layout) reliability making an echoo test. (For example a pc program would continuously send a serial frame and expect the echo from the board).

 

Is available an example implementing a similar feature, or better, is there a BAREMETAL project implementing the USB Serial Class Device? If not, do you know from where to start?

 

Thanks in advance to whom could give me some hints on how to implent such a feature.

Best Regards

 

G.

Outcomes