Pciexpress slave on imx6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Pciexpress slave on imx6Q

637 Views
Selea
Senior Contributor I

DEar Sir,

the PCiexpress peripheral on imx6,could be master or slave, but what i see is that the linux driver use it only as a master... Is it available also something to use it as a slave?

The basic idea is to cluster at least two imx6Q ...

Any other idea to do that?

Thanks

Omar

Labels (6)
0 Kudos
2 Replies

484 Views
Selea
Senior Contributor I

I read that two RC (master) on PCIe could be "connected" using a not trasparent PCIe switch.. Anybody used such solution? Or can confirm me that it could works?

Thanks

Omar

0 Kudos

484 Views
SergioSolis
NXP Employee
NXP Employee

Hello Omar,

You would need to modify the driver to set it as slave.

0 Kudos