Unable to use Rotary A& B as I2C pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to use Rotary A& B as I2C pins

500 Views
Nagraj
Contributor I

The default I2C pins can be initialized , but while trying to use the ROTARY A&B pins as the I2C CLK and DATA pins it is not able to initialize?

Can somebody help me in adding the I2C to the platfrom data as gpio ?

COMMAND BEING USED is shown below

noinitrd console=ttyAM0,115200 ubi.mtd=1 root=ubi0:rootfs0 rootfstype=ubifs rw gpmi

Labels (1)
0 Kudos
1 Reply

424 Views
SergioSolis
NXP Employee
NXP Employee

Hello Nagaraju,

I'm sorry, I don't quite understand what you are trying to do, what are you trying to achieve with the command you are using?

0 Kudos