The latest version of my header for this part "MK60D10.h" does not seem to have access to reset cause register SRSL. Indeed the same for the RM. For other versions of the K series you can read reset cause from SRSL.
Extract from header version:
** | Reference manual: | K60P144M100SF2V2RM Rev. 2, Jun 2012 |
** | Version: | rev. 1.8, 2013-06-24 |
I need to read back the reset cause. Any ideas?
Thanks
Ciarán Mac Aonghusa.
Solved! Go to Solution.
The System Register Status is defined in the header file as SRS0 and SRS1, check it out so you can correct your code and let me know if I can help you with something else.:smileyhappy:
The System Register Status is defined in the header file as SRS0 and SRS1, check it out so you can correct your code and let me know if I can help you with something else.:smileyhappy:
Thank you Perla Andrea.