AnsweredAssumed Answered

Kinetis I2S connexion to PCM

Question asked by Jordi Mercader on Sep 10, 2013
Latest reply on Sep 12, 2013 by Carlos Neri

We are trying to connect the audio bus from the Sierra wireless module SL6087 (PCM) with the I2S peripheral from Kinetis.

 

The hardware we are using is an eval board from Sierra wireless connected to the K60N512 tower through a level shifter board using the attached schematic.

 

The Sierramodule has the attached specifications, It only works as a master, bit serialclock 768kHz, transmits on Slot0 16bit word, with a frame sync of 8kHz.

 

We want to know the configuration of the SSI_LDD component from processor expert or non-processor expert solution code to be able to receive data from the Sierra module.

 

Best regards

Jordi

Attachments

Outcomes