Hello
I want to capture the video using parallel camera available on i.MX6Q SDP board and encode it with H.264 encoder and Mp4 as demuxer. I want to store that .mp4 file on SD card.
I have tried with following gst command but it is not working.
gst-launch mfw_v4lsrc fps-n=15 capture-mode=4 ! queue ! vpuenc codec=6 ! mp4mux ! filesink location=out.mp4 sync=false
I have tried to play .mp4 file on board using below command
gst-launch playbin2 uri=file:///out.mp4
it does not display anything either on PC or on board.
SO it looks that Mp4mux is not working.
After that i have tried to encode it using matroskamux using below command.
gst-launch mfw_v4lsrc fps-n=15 capture-mode=4 ! queue ! vpuenc codec=6 ! matroskamux ! filesink location=output.mkv sync=false
and try to play it using play2bin command and it played fine on board but it fails to play on PC using VLC media player.
Can anyone help me to get the .mp4 encoding working with mp4mux pipeline?
Please help on this issue.
Thanks,
J.
Can you enable logging (GST_DEBUG=*:2 before running the pipeline) and share it?
Leo