AnsweredAssumed Answered

Error in fsl-image-gui: qt4-x11-free_4.8.5.bb,  do_configure

Question asked by Leonardo Assad on Aug 31, 2013

Hi,

 

First, excuse me my bad english.

 

I am trying to learn how to use yocto and I am having problems with qt4-x11-free.

 

I am trying to compile fsl-image-gui but its stop with this error:

 

| collect2: error: ld returned 1 exit status

| make: *** [opengles2] Error 1

| OpenGL ES 2.x disabled.

| The OpenGL ES 2.0 functionality test failed!

|  You might need to modify the include and library search paths by editing

|  QMAKE_INCDIR_OPENGL_ES2, QMAKE_LIBDIR_OPENGL_ES2 and QMAKE_LIBS_OPENGL_ES2 in

|  /home/leonardo/Downloads/fsl-community-bsp/build/tmp/work/wandboard_quad-poky-linux-gnueabi/qt4-x11-free/4.8.5-r0/qt-everywhere-opensource-src-4.8.5/mkspecs/linux-gnueabi-oe-g++.

 

(...)

 

Task 418 (/home/leonardo/Downloads/fsl-community-bsp/sources/poky/meta/recipes-qt/qt4/qt4-x11-free_4.8.5.bb, do_configure) failed with exit code '1

NOTE: Tasks Summary: Attempted 3033 tasks of which 3028 didn't need to be rerun and 1 failed.

Waiting for 0 running tasks to finish:

 

Summary: 1 task failed:

  /home/leonardo/Downloads/fsl-community-bsp/sources/poky/meta/recipes-qt/qt4/qt4-x11-free_4.8.5.bb, do_configure

Summary: There was 1 ERROR message shown, returning a non-zero exit code

 

 

Can someone give me any help ?

 

Thanks.

 

Build Configuration:

BB_VERSION        = "1.19.1"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-13.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "wandboard-quad"

DISTRO            = "poky"

DISTRO_VERSION    = "1.4+snapshot-20130831"

TUNE_FEATURES     = "armv7a vfp neon callconvention-hard cortexa9"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "(nobranch):d63e6a925a78f0f5fb7e7329b5cc2993f1ec9b14"

meta-oe           = "(nobranch):72e23c12296fbc77193898c38426add58d0c2d71"

meta-fsl-arm      = "(nobranch):13c91f33e30ab1c0d2a20e414753008bbdabca95"

meta-fsl-arm-extra = "(nobranch):69bed23e70f84ff9a67b9a416f588a98fb72aa1e"

meta-fsl-demos    = "(nobranch):d38f95c8f5c12c8fa38c962daf7190dba1915672"

Original Attachment has been moved to: yocto-error.txt.zip

Outcomes