Hi Community,
I´m a newbei in the U-boot development, nowadays I try to create a U-boot for a custom board based in iMX6Q from freescale. I have been understanding the IOMUX files and program and also the GPIO register in that board, because I would like to set a led during the U-boot connected in the GPIO5_15 in the board like it is in the SabreAI Card as default.
I have configured the Iomux to select the GPIO function in the ball T20 of the iMX6Q with the following description in the PAD_DISP0_DAT21:
writel((SION_DISABLED & 0x1) << 4 | (ALT5 & 0x7), IOMUXC_SW_MUX_CTL_PAD_DISP0_DAT21);
writel((HYS_ENABLED & 0x1) << 16 | (PUS_100KOHM_PU & 0x3) << 14 | (PUE_PULL & 0x1) << 13 |
(PKE_ENABLED & 0x1) << 12 | (ODE_DISABLED & 0x1) << 11 | (SPD_100MHZ & 0x3) << 6 |
(DSE_40OHM & 0x7) << 3 | (SRE_SLOW & 0x1), IOMUXC_SW_PAD_CTL_PAD_DISP0_DAT21);
I have seen that when the pins works like a GPIO, they have a extra registers that they are independent of the IOMUX configuration (Reference: Chapter 28 in the iMX6Q Data sheet). If I am not wrong, to work like a output the GPIO5_15 and the led will be on. I need to set the following registers:
My question If it is possible to make in the U-boot and whether it is, which is the correct file to do that. I tried to change the c file from the board in <u-boot directory>/<board>/<directory of my custom board>/<name_of_the_board>.c.
in the function board_init. The changes in that function are the following:
writel((1 & 0xffffffff ) << 15, GPIO5_BASE_ADDR + GPIO_GDIR);
writel((1 & 0xffffffff ) << 15, GPIO5_BASE_ADDR + GPIO_DR);
Although that could be work, I am still thinking that it is a complety wrong system to develop a correct U-boot for my custom board.
Any help will be gratefully,
-Regards
Solved! Go to Solution.
You don't need to access the GPIO registers directly. There is a GPIO API you can use.
Check for example: board/wandboard/wandboard.c
static void setup_iomux_enet(void)
{
imx_iomux_v3_setup_multiple_pads(enet_pads, ARRAY_SIZE(enet_pads));
/* Reset AR8031 PHY */
gpio_direction_output(ETH_PHY_RESET, 0);
udelay(500);
gpio_set_value(ETH_PHY_RESET, 1);
}
You don't need to access the GPIO registers directly. There is a GPIO API you can use.
Check for example: board/wandboard/wandboard.c
static void setup_iomux_enet(void)
{
imx_iomux_v3_setup_multiple_pads(enet_pads, ARRAY_SIZE(enet_pads));
/* Reset AR8031 PHY */
gpio_direction_output(ETH_PHY_RESET, 0);
udelay(500);
gpio_set_value(ETH_PHY_RESET, 1);
}
Hi Fabio,
Thanks for your answer, now I have a reference to follow.
-Regards