AnsweredAssumed Answered

libvivante-dfb-mx6 no found issue on yocto

Question asked by Mark Lee on Aug 21, 2013
Latest reply on Feb 24, 2014 by Yixing Kong

Hello Guys,

 

I am trying to enable wayland function on i.MX6 sabre auto board with yocto alpha release (git://git.freescale.com/imx/meta-fsl-bsp-release.git, dylan_3.5.7-1.0.0 branch). I am using fsl-image-dfb-sdk image, and following the wiki page, https://wiki.yoctoproject.org/wiki/Wayland to enable wayland, but may meet an error as below. It seems libvivante-dfb-mx6 can not found when doing rootfs. Does someone meet the same issue or how should I fix the issue?

 

Parsing recipes: 100% |#############################################################################################################################################################################| Time: 00:00:51

Parsing of 1471 .bb files complete (0 cached, 1471 parsed). 1844 targets, 74 skipped, 0 masked, 0 errors.

 

Build Configuration:

BB_VERSION        = "1.18.0"

BUILD_SYS         = "x86_64-linux"

NATIVELSBSTRING   = "Ubuntu-12.04"

TARGET_SYS        = "arm-poky-linux-gnueabi"

MACHINE           = "imx6qsabreauto"

DISTRO            = "poky"

DISTRO_VERSION    = "1.4.1"

TUNE_FEATURES     = "armv7a vfp neon"

TARGET_FPU        = "vfp-neon"

meta             

meta-yocto        = "(nobranch):e4a0a4c5e419154a34710a1b6c28d4180c6304c3"

meta-browser      = "dylan:2140f2a114f7009f86479afb12a524bb157cbb0e"

meta-oe          

meta-gnome        = "(nobranch):13ae5105ee30410136beeae66ec41ee4a8a2e2b0"

meta-fsl-arm      = "(nobranch):d31a4e85673874dbc6b42bb5d1e8496810c574cc"

meta-fsl-arm-extra = "(nobranch):5f5a9cfcad223f5a1c623346780510ffcdc012ab"

meta-fsl-demos    = "(nobranch):724cfb929748f47782dea3b1dc412b028f6f3515"

meta-fsl-arm     

meta-fsl-demos    = "(nobranch):7c9369b7a80276c438439f1a79b86e32721630b0"

 

NOTE: Resolving any missing task queue dependencies

NOTE: multiple providers are available for jpeg (jpeg, libjpeg-turbo)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg

NOTE: multiple providers are available for jpeg-native (jpeg-native, libjpeg-turbo-native)

NOTE: consider defining a PREFERRED_PROVIDER entry to match jpeg-native

NOTE: Preparing runqueue

NOTE: Executing SetScene Tasks

NOTE: Executing RunQueue Tasks

WARNING: perf: The compile log indicates that host include and/or library paths were used.

         Please check the log '/workspace/work/ubuntu12.04/w20_fsl_wayland/Yocto_Alpha/fsl-community-bsp/build_wayland_dfb_sdk/tmp/work/imx6qsabreauto-poky-linux-gnueabi/perf/1.0-r8/temp/log.do_compile' for more information.

ERROR: Function failed: do_rootfs (see /workspace/work/ubuntu12.04/w20_fsl_wayland/Yocto_Alpha/fsl-community-bsp/build_wayland_dfb_sdk/tmp/work/imx6qsabreauto-poky-linux-gnueabi/fsl-image-dfb-sdk/1.0-r0/temp/log.do_rootfs.30334 for further information)

ERROR: Logfile of failure stored in: /workspace/work/ubuntu12.04/w20_fsl_wayland/Yocto_Alpha/fsl-community-bsp/build_wayland_dfb_sdk/tmp/work/imx6qsabreauto-poky-linux-gnueabi/fsl-image-dfb-sdk/1.0-r0/temp/log.do_rootfs.30334

Log data follows:

| DEBUG: Executing shell function do_rootfs

| Note: configuring RPM platform settings

| Note: configuring RPM system provides

| Note: configuring RPM DB settings

| Note: configuring Smart settings

|

|

|

|

|

|

| Note: adding Smart channel imx6qsabreauto (60)

|

|

| Note: adding Smart channel cortexa9hf_vfp_neon (55)

|

|

| Note: adding Smart channel all (10)

|

|

| Note: configuring RPM cross-install scriptlet_wrapper

|

| Updating cache...               ######################################## [100%]

|

| Saving cache...

|

| Error: libvivante-dfb-mx6 not found in the base feeds (imx6qsabreauto cortexa9hf-vfp-neon cortexa9hf-vfp armv7ahf-vfp-neon armv7ahf-vfp armv6hf-vfp armv5ehf-vfp armv5hf-vfp noarch any all).

| ERROR: Function failed: do_rootfs (see /workspace/work/ubuntu12.04/w20_fsl_wayland/Yocto_Alpha/fsl-community-bsp/build_wayland_dfb_sdk/tmp/work/imx6qsabreauto-poky-linux-gnueabi/fsl-image-dfb-sdk/1.0-r0/temp/log.do_rootfs.30334 for further information)

ERROR: Task 7 (/workspace/work/ubuntu12.04/w20_fsl_wayland/Yocto_Alpha/fsl-community-bsp/sources/meta-fsl-bsp-release/imx/meta-fsl-demos/recipes-fsl/images/fsl-image-dfb-sdk.bb, do_rootfs) failed with exit code '1'

 

Thanks and best regards,

Mark Lee

Outcomes