I am laying out a prototype board for the MKE02Z64VQH2 (64 pin package). I want to use both SPIs, but the reference manual seems to have an error. SPI0_MOSI is shown on pin 31 and 59. SPI0_SCK is shown on pins 32 and 60. I do not see a SPI1_SCK, SPI1_MOSI.
Any ideas of the correct pinout?
Solved! Go to Solution.
Hi Donald,
In the datasheet on the KE02 website, it lists SPI1_SCK on pin 2 and SPI1_MOSI on pin 1. I also checked the RM, and it's in there as well. Perhaps you had an older version of the materials that was missing that information.
-Anthony
Hi Donald,
In the datasheet on the KE02 website, it lists SPI1_SCK on pin 2 and SPI1_MOSI on pin 1. I also checked the RM, and it's in there as well. Perhaps you had an older version of the materials that was missing that information.
-Anthony
Oops, you are correct.
I was looking at Alt 2 where the rest of the SPI pins were configured, not at Alt 3.
Thank you,
Don Porada