por favor necesito unos ejemplos de control de servo con el jm60, que se mueva de 0 grados a 90 espere un tiempo y se devuelva a 0.
---------------------------------
please I need some examples of servo control with jm60, moving from 0 to 90 degrees, waits for some time and returns to 0.
Message was edited by: Monica Arvizu
Hello,
Please can you provide us more details regarding your problem ?
We need to know exactly what is the tool version you're using.
To do that you must:
Under CodeWarrior IDE (classic)
Start the IDE and click on Help | About Freescale CodeWarrior.
Click on Installed Products
Provide us all info displayed.
Or you can save them in a txt file.
Under Eclipse IDE
1- Start Eclipse and click on Help ¦ Freescale Licenses
The Status column gives the status of the license.
Under Product, select it and click on details.
A new dialog show up giving license details.
Provide us all info displayed
2- Start Eclipse and click on Help ¦ About CodeWarrior Development Studio
Under Installed Products, you will see the version used.
If the Installed Products is not available for older version you should find information in the welcome.txt
under the installation folder.
what is the processor and interface used ?
regards
Pascal