Error import project in CW10.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error import project in CW10.4

Jump to solution
559 Views
kappa74
Contributor IV

Good morning,

I'm passing from CW10.2 to CW10.4.

I installed CW10.4 but and then I imported the project in the nwe workspace.

When I import the project I get always the error:

"An internal error has occurred.

String index out of range: -1"

5750_5750.pngpastedImage_0.png

 

Which string is in error?

Why do I get it?

Thank you

Best Regards

Mirko

Labels (1)
0 Kudos
1 Solution
391 Views
kappa74
Contributor IV

I attached the 2 files project

View solution in original post

0 Kudos
2 Replies
391 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

can you upload your project for us to check?

0 Kudos
392 Views
kappa74
Contributor IV

I attached the 2 files project

0 Kudos