AnsweredAssumed Answered

CW 10.2 App fails to compile after conversion to CW 10.4

Question asked by Hugues Leger on Aug 20, 2013
Latest reply on Sep 4, 2013 by ZhangJennie

I imported a 10.2 project into CW 10.4; now the application will not compile. The application is set up to create an s-record as output. I found out unless I specify and extension for the build artifact (Propeties->C/C++ Build->Settings) in the Build Articat tab, or add a dot (.) to the Artifact name (e.g. console.flash), the project will not compile.  When in Properties->Settings->ColdFire Linker->Output window, the Generate S-Record File box is checked, the artifact extension must remain blank as the s19 extensition will automatically be added to the file name.  Has anyone else run into this problem with CW 10.4? Does anyone know if this issue is being addressed in CW 10.4.2?

Outcomes