MMPF0100 how to enter OFF mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MMPF0100 how to enter OFF mode

693 Views
peterhygren
Contributor III

We've developed a custom board with IMX6D and MMPF0100 (default version) and are running a yocto custom build. We have a problem with power off mode, we can't enter it. We're not interested in sleep or standby etc.

The datasheet for MMPF0100 states that if PWRON is set low and SWxOMODE bits are not set, OFF mode should be entered, however the voltages (SW1-4 and VGEN1-6) won't shut off so I assume sleep is entered. However I am seeing some weird behavior in SW2, namely it alternates between 1.8V and 2.2V.

The power button is connected to the CPU and I see no difference between "shutdown -h 0" and just asserting the power button for >4s.

Any ideas?

Labels (4)
0 Kudos
0 Replies