AnsweredAssumed Answered

K60 Bootload via AN4367... Stupid Question

Question asked by snowkid on Aug 16, 2013
Latest reply on Aug 22, 2013 by snowkid

Great Ap Note... Coded into two designs... works like a champ!

 

So here's my stupid question:  How come this works????

 

This approach to bootload involves executing and programing Flash memory in the K60 all confined to Block 0. How is it that I am not seeing read while write issues??? 

See this from AN4367 (note, the application itself is loaded into 0x0000_C0000):

 

 

The bootloader is placed into the first 48 KB of the on-chip flash memory, but the actual size of the bootloader can be smaller. The user application can be placed into the flash area above the bootloader flash area. The last 4 KB of the flash memory must be reserved for the bootloader's parameters storage, which is defined by the size of the erase-page of the on- chip flash memory.

The following figure shows the memory map and the bootloader memory footprint. The bootloader code is located in the first address of the flash memory, 0x0000_0000 to 0x0000_BFFF. The bootloader parameters are located in the first address of the last logical-block of the flash memory, 0x0007_F000 to 0x0008_0000 (in Kinetis MK60n512).

bootmap.jpg

 

 

Outcomes