Hi, I get this error kicked out of the console after running my post-build windows cmd script. It's seems to be a Windows 7 command line error, like when you try to copy files with embedded spaces etc. I can run my cmd script from the command line with no error, even checking that %errorlevel% is zero. Everything works except this annoying message at the end. If I remove the post-build entry, I do not get the error. The "All Done!" is echoed from the cmd script. After that CW10.3 takes over.
Thanks,
John Reynolds
.
.
.
C:/Freescale/CW MCU v10.3/gnu/bin/mingw32-make --no-print-directory post-build
'Generate CRC and append to .rbin '
MQXbootPost C:/Freescale/Freescale_MQX_4_0/demo/Windchime\twrcf52259_Int_Flash_Bootloader_Debug Windchime.elf.rbin
Windchime.elf.rbin is 524288 bytes
Read 516094 bytes starting at 0x2000. CRC=0xEFA6
03:41 PM
All done!
' '
Hi John,
could you please post your script in this thread for investigating?
if possible, could you please also post your project here also?