AnsweredAssumed Answered

TFTP Client "PUT" operation?

Question asked by Chris Paynter on Aug 13, 2013

I'm running MQX 4.01, looking at the RTCS demo project, specifically the TFTP client, running on a TWR-K60N512.  As far as I can see, it only supports reading a file from a remote server, not writing one to the server.  Anybody ever find a way to do this?

 

The shell command Shell_TFTP_client() in sh_tftp.c has a comment in the function header which hints that it will "TFTP to or from a host", but I don'd see any way to do it from there.  tftp.c seems only to support "get" operations with function TFTP_read().

 

thanks!

Chris

Outcomes