AnsweredAssumed Answered

Issue entering the U-Boot prompt mode.

Question asked by swl on Aug 6, 2013
Latest reply on Feb 24, 2014 by Yixing Kong
Branched to a new discussion

Hi,

 

I am trying to run an image on the target but encountered some difficulties in entering the U-Boot prompt.

 

I first attempted to download the image using MFQTool in SD3 boot mode.

 

cfg.ini

 

{LIST}

name=ubuntu-SabreSD-eMMC

 

 

After downloading Images using MFQTool, i switch back to eMMC4.4 boot mode.

When i restart the board, I'm not able to see the count down timer for me to enter the U-Boot prompt.

I get the following instead.

 

UBoot 2009 08 (Apr 25 2013 - 01:17:52)

..

..

..

Board:i.Mx^Q-SABRESD: unknown-board Board:0x63012 [ POR ]

Boot Device: MMC

I2C: ready

DRAM: 1GB

MMC: FSL_USDHC:0, FSL_USDHC:2, FSL_USDHC:3

 

 

if anyone has encountered similar situation or has a solution for it, please share it with me.  Thanks

Outcomes