Hi all,
With the i.MX28 Windows CE BSP the touch screen calibration is launched every time on startup (touchc.exe). I need to modify touchc.exe so that the calibration screen is only presented if there is not already a valid calibration in the registry.
touchc.exe is provided pre-compiled in the 'files' folder within the various OS templates.
Does anyone have the source for touchc.exe so I can edit it to check the registry for existing calibration data?
Kind regards,
Mark
1.
Sorry, we do not have “touchc.exe” sources.
Seems, You need to apply to Microsoft.
2.
The following was found in I-net, and seems, is working.
Platform Builder can automatically clone TouchCalibrate:
1. Open your Workspace
2. From the catalog, search for <Minimal GDI Configuration>
3. Right click and choose <Clone Catalog Item>
4. A bunch of libraries will be listed, but the one you want is <calibrui>.
Make sure it is checked and select <OK>.
This puts a copy of TouchCalibrate in the directory "calibrui" in your workspace.
You can now change […] the code and this will replace the standard function.”