LPDDR2 Configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPDDR2 Configuration

Jump to solution
1,070 Views
jonpartee
Contributor I

What do the TINIT, TINIT3, TINIT4, TINIT5 in the DDR_CR02-DDR_CR05 Correspond to in reference to LPDDR2 data sheet.  The latest reference manual has little/no information on this.  Not all of the LPDDR2 datasheets label the INIT times the same.

Jon

Labels (4)
Tags (2)
0 Kudos
1 Solution
604 Views
ioseph_martinez
NXP Employee
NXP Employee

Yes, seems the manual is lacking from that information.

TINIT: Defines the DRAM initialization delay, in memory clocks.(time required for memory clocks to be started and stabilized before clock enable becomes active)

TINIT3: Defines the number of memory clocks required from CKE assertion to memory reset. (this parameter only applies when the controller is configured for LPDDR2)

TINIT4: Defines the number of memory clocks required from memory reset to an MRR command (this parameter only applies when the controller is configured for LPDDR2)

TINIT5: Defines the maximum number of memory clocks required from memory reset to initialization complete (this parameter only applies when the controller is configured for LPDDR2)


AlejandroSierra, you may be interested on this...

View solution in original post

0 Kudos
1 Reply
605 Views
ioseph_martinez
NXP Employee
NXP Employee

Yes, seems the manual is lacking from that information.

TINIT: Defines the DRAM initialization delay, in memory clocks.(time required for memory clocks to be started and stabilized before clock enable becomes active)

TINIT3: Defines the number of memory clocks required from CKE assertion to memory reset. (this parameter only applies when the controller is configured for LPDDR2)

TINIT4: Defines the number of memory clocks required from memory reset to an MRR command (this parameter only applies when the controller is configured for LPDDR2)

TINIT5: Defines the maximum number of memory clocks required from memory reset to initialization complete (this parameter only applies when the controller is configured for LPDDR2)


AlejandroSierra, you may be interested on this...

0 Kudos