i.MX6q Android going to suspend on bootup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6q Android going to suspend on bootup

1,442 Views
Trilokesh
Contributor I

Hi All,

 

Please help in resolving the issue of suspending the CPUs'.

When I poweron the boot process goes smooth and after boot it is suspending the CPUs

 

Throws the following prints.

 

Freezing user space processes ... (elapsed 0.02 seconds) done.

Freezing remaining freezable tasks ... (elapsed 0.01 seconds) done.

add wake up source irq 51

PM: suspend of devices complete after 120.017 msecs

PM: late suspend of devices complete after 0.652 msecs

Disabling non-boot CPUs ...

CPU1: shutdown

CPU2: shutdown

CPU3: shutdown

 

The attached is the full log from logcat. I'm using a custom hardware where I don't have any buttons to configure for wakeup.

 

I'm stuck here. Please help me to resolve.

 

Thanks to all.

Original Attachment has been moved to: imx6q_android_4.2.2_logcat.txt.zip

0 Kudos
5 Replies

668 Views
YixingKong
Senior Contributor IV

Trilokesh

This discussion is closed since no activity. If you still need help, please feel free to reply with an update to this discussion, or create another discussion.

Thanks,

Yixing

0 Kudos

668 Views
YamilGarcia
Contributor III

Hi,

Can you share your kernel cmdline?

Regards,

Yamil

0 Kudos

668 Views
Trilokesh
Contributor I

Hi Yamail garcia,

the below is my command line arguments.

Kernel command line: console=ttymxc3,115200 calibration enable_wait_mode=off no_console_suspend androidboot.hardware=freescale androidboot.console=ttymxc3  init=/init vmal

loc=256M video=mxcfb0:Primeview-PM070WL4,bpp=32 fbmem=10M,28M video=mxcfb1:hdmi,1280x1024M@60,bpp=32 if=RGB24 vt.global_cursor_default=0 consoleblank=0 board_mx6q_phyflex.csi0=none board_mx6q_phyflex.csi1=none ip=none root=/dev/mmcblk0p2 rootfstype=ext4 noinitrd rootwait mtdparts=n25q128:512k(barebox)ro,128k(bareboxenv),2M(splash),-(kernel);gpmi-nand:512k(barebox)ro,128k(bareboxenv),2M(splash),8M(kernel),-(root)

0 Kudos

668 Views
YixingKong
Senior Contributor IV

Trilokesh

We have not got your response yet and will close the diacussion in 3 days.

Thanks,

Yixing

0 Kudos

668 Views
admin
Specialist II

Did you ever get your suspend issue resolved, or is it still an issue for you?

0 Kudos