AnsweredAssumed Answered

web_hvac runs fine on TWR-K70, but gives 'Out of Memory' task errors

Question asked by Gene Goff on Jul 30, 2013
Latest reply on Aug 2, 2013 by Martin Latal

The web_hvac Demo project straight from MXQ 4.0 runs fine on the TWR-K70 system, but if I suspend execution and look at the MQX Task Summary, the TCP/IP and httpd server tasks always have a Task Error Code of 'Out of Memory (0x0004), even if the program only runs a few seconds and I never request a web page.  Anyone know what is causing this and how to increase the memory allocated to these two tasks?  The stack for these tasks has not overflowed, so it is not out of stack memory.  The RTCS_MINIMUM_FOOTPRINT is defined by default as this project comes, which gives _RTCSPCB_max = 20 which seems plenty, and increasing to 40 makes no difference.

Outcomes