A problem with kinetis K20 IAP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

A problem with kinetis K20 IAP

589 Views
yuting
Contributor I

i want to wite an IAP bootloader  for K20(refer to an2295sw). I can erase program flash sector and wirte a long word into program flash sector. but if i sequentially write several long bytes. it will cause Resetting the chip. In fact, when i earase a program flash sector ,it cause resetting too.

(I operate FCCOB registers using Program Section Command and Program Longword Command)

Thanks in advance,

yuting.

Tags (3)
0 Kudos
1 Reply

343 Views
alejandrolozan1
NXP Employee
NXP Employee

Hi Yuting,

Can you provide mode details about your problem?

Does the device feature FlexNVM? Which commands are you using? Program Section?
Are the flash routines executing from RAM?

Best Regards,

Alejandro

0 Kudos