AnsweredAssumed Answered

MQX 4.0.1 RTCS examples not working

Question asked by Nathan Kohler on Jul 26, 2013
Latest reply on Jul 28, 2013 by TomE

I was using MQX 3.7 with CodeWarrior 10.2 without any problems on my M52259EVB.

 

I downloaded and installed MQX 4.0.1 and compiled all the libraries using the default user_config.h and default linker files.  I then built several example projects.

 

All of the RTCS and MFS example projects crash with "

***UNHANDLED INTERRUPT ***

Vector#: 0     0x00

 

It seems to occur right when RTCS_create() is called.  Other projects like the flashx, hello world, and some shell examples run without any problems.

 

Is there something I need to change in the user_config.h file to get the RTCS and MFS examples to run?

 

edit:  This is using the intflash Release build configuration.  All libraries and projects built and linked without issue.

 

Thanks,

 

Nate

Outcomes