The OS is windows XP, double click the application file to install, and it come out nothing.
But other computer with Win7 OS can install it and work propertly. Do you have this problem?
Solved! Go to Solution.
The FreeMASTER application requirements can be easily satisfied by almost any Windows-based host PC available today. It was tested with the latest version of Microsoft Windows XP and Windows 7.
Are you using version 1.3.16, which can be downlaoded from:
The FreeMASTER application requirements can be easily satisfied by almost any Windows-based host PC available today. It was tested with the latest version of Microsoft Windows XP and Windows 7.
Are you using version 1.3.16, which can be downlaoded from:
I download the same version, but the problem is, when I double click the application program, then there is no response, my colleague has also attempt to install it, can’t either. My OS maybe not the latest version of XP