AnsweredAssumed Answered

Need help re configuring Ethernet support for i.MX35

Question asked by Jam Hub on Jul 17, 2013
Latest reply on Jul 17, 2013 by Yuri Muhin

Standard  Linux 2.6.31 from Freescale is used to date. The default config supports

the i.MX35 3 stack board including the debug board with UART and Ethernet. Everything

works well.


Now trying to switch to Personality Board + CPU board only configuration.

It has a different SMSC LAN8700 chip. The Debug board has LAN9217.

 

Has anybody used this configuration and what are the changes that need to be

done for Uboot and Linux in order to support this Ethernet port?  Also, if an

external RS232 dongle is used connecting to the UART1 pins on the 500 pin connector

- are there code changes required for that, or existing code should work as is?

 

Thanks in advance,

 

 

Outcomes