Hi,
I have an touchscreen and an HDMI monitor connected to the board, the screens are mirrored. From a Linux/Android point of view, I can access (read/write) to fb0 and fb1 independently. But I was wondering if it's possible to render something in OpenGL only on fb1 ?
Thanks in advance for your help.
Yes, you can use any of the FB0 and FB1
In the source code should be a call like this:
EGLNativeWindowType native_window = open("/dev/fb0",O_RDWR);
Where it specifies what FB to use, here is where you can change to other FB