i.MX6Q CAN Chip Errata ERR05829

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6Q CAN Chip Errata ERR05829

Jump to solution
645 Views
wayne_s
Contributor II

Does anyone know if the FlexCAN driver in the linux bsp has the workaround implemented as described in ERR05829?  The note says that there is no software workaround available, but a workaround is presented in the document.

Regards,

Wayne

Labels (4)
Tags (1)
0 Kudos
1 Solution
490 Views
SergioSolis
NXP Employee
NXP Employee

Hello Wayne,

No, it is not implemented. You need to implement it until the fix is available.  The instructions on the workaround are in the errata.

View solution in original post

0 Kudos
1 Reply
491 Views
SergioSolis
NXP Employee
NXP Employee

Hello Wayne,

No, it is not implemented. You need to implement it until the fix is available.  The instructions on the workaround are in the errata.

0 Kudos