I am looking for example code for using the IntEEPROM. I realize it is processor dependent but it looked straight forward in use. Using an S08PA16, figured we would keep one MCU vendor in house instead of 3.
Looking for setup/use for GetWord and SetWord. We generate nothing but errors in our short experiment.
Bill
Hi William,
Did you got success in your application using EEPROM of S08PA16?
I'm trying to solve the same problem.
If it's possible, could you send me the example you did?
Thanks a lot.
Edson
Thanks Vojtech. I have become so used to ferreting information I forgot the obvious place.
Did notice all the examples are in byte format, Just adjusted it for word and got error that it was looking for a byte, odd.
Thanks again.
Hello,
in case the problem persist, could you please post here some project demonstarting the behaviour?
Best regards
Vojtech Filip
Processor Expert Support Team
I'm also having problems using the IntEEPROM functions with my MC9S08PT60 MPU.
I've tried contacting Freescale support a week ago regarding it(Service Request "SR 1-2057880684"), but I havent got any response yet...
First I think I've found two errors in the PE generated code:
1. "typedef byte * IEE1_TAddress; /* Type of address to the EEPROM */ "
in the file IEE1.h needs to be a pointer to a word not a byte (since the eeprom address starts at 0x3100)
2. This row in both the functions IEE1_GetByte and IEE1_SetByte seams to be wrong
" if(((word)Addr <...." It should start with "if(((word)*Addr <..... " otherwise it compares the adress of the pointer and not the adress itself.
(It's a little annoying to change this back every time I've regenerated the PE-code, any ideas on how to avoid that?)
But even after fixing these, I still can't write to the eeprom area.
I get the error code "9" (ERR_NOTAVAIL), and when I debug it I can see that it is the function EraseSectorInternal() that is called from the IEE1_SetByte()-function that generates the error code.
I then started to look at the registers, and it gives the errorcode because the bit ACCERR in the status register NVM_FSTAT is set.
I've made a test project to debug it and to highlight the problem:
https://www.dropbox.com/s/0h2tks5ybo2mtpu/eeprom_test.zip
It's written for a TWR-SO8PT60 kit, and requires a serial cable to the computer.
It reads a character that you send from a hyperterminal window (9600,8,N,1,N)
Then the program tries to store it to the eeprom-area
and then retreive it and echo it back to the terminal window together with some debug info.
It also displays the error codes and the status of the NVM_FSTAT register.
The read functions seems to work (it returns "1" all the time, but no error codes)
I get this result in the terminalwindow:
Error code(after eeprom write):09
NVM_FSTAT(after eeprom write): 10100000
Error code(after eeprom read): 00
stored character echoed back: 1
I'm using codewarrior 10.6
I've tried to both enable and disable Memory area 5 in build options for the cpu.
And both exclusive eeprom usage and not for the intEEPROM-component
And both safe and destructive writes.
The MCU:s both in my tower-kit and in the actual prototype I'm working on are of the 4N40C batch btw.
In case this is another bug in the hardware...
Can anyone please help me out?
Hi,
With the help of Willian and people from our representative and distribuitor for Freescale, ITECH, I got success using INTEEPROM.
See below my code:
#include "IEE1.h" // this must be in the beginning of the program
Main()
{
Sinal = 10;
Vmin1Sinal = 11;
Vmax1Sinal = 12;
IEE1_SetWord(IEE1_AREA_START, Sinal); //save first 16 bits variable
IEE1_SetWord(IEE1_AREA_START+2,Vmin1Sinal); //save second 16 bits variable
IEE1_SetWord(IEE1_AREA_START+4, Vmax1Sinal); //save third bit variable
IEE1_GetWord(IEE1_AREA_START, &POT1min); //read first position and save in variable POT1min
IEE1_GetWord(IEE1_AREA_START+2,&POT1max); // read second position and save in variable POT2max
IEE1_GetWord(IEE1_AREA_START+4,&POT2min); // read third position and save in variable POT2min
}