AnsweredAssumed Answered

DFI FS200-M53 BOOT HELP!

Question asked by matz spitz on Jul 8, 2013
Latest reply on Jul 10, 2013 by 4guin4g4

Hello,

 

NOOBIE QUESTION

 

I recently got ahold of a DFI FS200-M53 which uses the i.MX53 freescale chipset. It ships with android, but I wanted to put Ubuntu server on it. There is a special image which I have to install Ubuntu.

 

When I plug in the board via the OTG USB into windows 7 I get a driver issue says "MX53 SMD Android" not found. I try to open up MFGtool but it doesn't work.

 

How can I change the OS on this board to Ubuntu?

 

Please help

 

Thanks,

Outcomes