AnsweredAssumed Answered

Could not recieve data on UART4

Question asked by Kopera Pune on Jul 8, 2013
Latest reply on May 25, 2014 by Boris-Ben Shapiro
Branched to a new discussion

I am trying to configure UART4. I have added

MX6SL_PAD_KEY_ROW6__UART4_TXD

and

MX6SL_PAD_KEY_COL6__UART4_RXD

in mx6sl_brd_pads[ ].

 

Above pin configs are defined as

#define MX6SL_PAD_KEY_ROW6__UART4_TXD                                         \

        IOMUX_PAD(0x04AC, 0x01A4, 1, 0x0000, 0, MX6SL_UART_PAD_CTRL)

      

#define MX6SL_PAD_KEY_COL6__UART4_RXD                                         \

        IOMUX_PAD(0x048C, 0x0184, 1, 0x0814, 2, MX6SL_UART_PAD_CTRL)

 

I crosschecked these configs and looks like these configs are correct..

 

I have also called "imx6sl_add_imx_uart(3,NULL)" from function mx6_evk_init()

 

I configured UART5 just same as UART4. UART5 works well where as UART4 sends data correctly however could not receive it.

 

Would you please provide me pointers to solve this problem.


Outcomes