I want to use two CSI the same time on sabre-lite(OV5642[Prallel] and OV5640[MIPI]).
Now only use a camera (OV5642 or OV5640) to capture video is OK.
I think it could use to each IPU.
So I modify
static struct fsl_mxc_capture_platform_data capture_data[] = {
{
.csi = 0,
.ipu = 0,
.mclk_source = 0,
.is_mipi = 0,
},
{
.csi = 0,
.ipu = 1,
.mclk_source = 1,
.is_mipi = 1,
}
};
but it not useful.
How should I go to put the camera on each IPU??? It can will work the same time.