Enabling Ethernet in SABRE SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Enabling Ethernet in SABRE SDB

Jump to solution
2,675 Views
vishvapathi
Contributor V

Hi,

I have booted my imx6 SABRE SDB evk from the sd card with Linux version 3.0.35-2508.  The eth0 is not working . the light of eth0 blinks periodically

root@freescale /$ ifconfig -a 

eth0 Link encap:Ethernet HWaddr 00:04:9F:02:6C:A6

  BROADCAST MULTICAST MTU:1500 Metric:1

  RX packets:0 errors:0 dropped:0 overruns:0 frame:0

  TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

  collisions:0 txqueuelen:1000 

  RX bytes:0 (0.0 b) TX bytes:0 (0.0 b)

 

lo Link encap:Local Loopback 

  LOOPBACK MTU:16436 Metric:1 

  RX packets:0 errors:0 dropped:0 overruns:0 frame:0

  TX packets:0 errors:0 dropped:0 overruns:0 carrier:0

  collisions:0 txqueuelen:0 

  RX bytes:0 (0.0 b) TX bytes:0 (0.0 b)


Labels (2)
0 Kudos
1 Solution
1,170 Views
vishvapathi
Contributor V

The linux kernel was without ethernet. Activated  by:

  ipconfig eth0 up                    // to load the FEC driver

  udhcpc                                // to obtain the IP address via DHCP when required.

and it works now..

thanks


View solution in original post

0 Kudos
7 Replies
1,170 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Vishvapathi,

      It seems that ethernet didn't get IP address. Did you add ip=dhcp in bootargs of u-boot environment ?

Regards,

Weidong

0 Kudos
1,170 Views
vishvapathi
Contributor V

Hi Weidong,

  Yes, i did set tht.. below is my env setting

MX6Q SABRESD U-Boot > printenv 

bootdelay=3 

baudrate=115200 

ipaddr=192.168.1.103 

serverip=192.168.1.101 

netmask=255.255.255.0 

loadaddr=0x10800000 

rd_loadaddr=(0x1300000) 

netdev=eth0 

ethprime=FEC0 

uboot=u-boot.bin 

kernel=uImage 

nfsroot=/opt/eldk/arm 

bootargs_nfs=setenv bootargs ${bootargs} root=/dev/nfs ip=dhcp nfsroot=${serverp

bootcmd_net=run bootargs_base bootargs_nfs; tftpboot ${loadaddr} ${kernel}; boom

ethact=FEC0 

bootargs_mmc=setenv bootargs ${bootargs} root=/dev/mmcblk1p1 rootwait rw init=/t

bootargs_base=console=ttymxc0,115200 

bootargs=console=ttymxc0,115200 setenv bootargs ${bootargs} root=/dev/mmcblk1p1t

bootcmd_mmc=mmc dev 2;mmc read ${loadaddr} 0x800 0x2000;bootm 

bootcmd=run bootcmd_mmc 

stdin=serial 

stdout=serial 

stderr=serial 

bootargs_base_mmc=root=/dev/mmcb1k1p1 rootfstype=ext3 rootwait rw ip=dhcp

root@freescale ~$ ifconfig eth0 up 

eth0: Freescale FEC PHY driver [Generic PHY] (mii_bus:phy_addr=1:01, irq=-1)

root@freescale ~$ PHY: 1:01 - Link is Up - 100/Full 

root@freescale ~$ ifconfig -a 

eth0 Link encap:Ethernet HWaddr 00:04:9F:02:6C:A6 

  UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1 

  RX packets:10 errors:0 dropped:0 overruns:0 frame:0 

  TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 

  collisions:0 txqueuelen:1000 

  RX bytes:640 (640.0 b) TX bytes:0 (0.0 b) 

 

lo Link encap:Local Loopback 

  LOOPBACK MTU:16436 Metric:1 

  RX packets:0 errors:0 dropped:0 overruns:0 frame:0 

  TX packets:0 errors:0 dropped:0 overruns:0 carrier:0 

  collisions:0 txqueuelen:0 

  RX bytes:0 (0.0 b) TX bytes:0 (0.0 b)


0 Kudos
1,170 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello,Vishvapathi,

      Would you like to try the following settings in u-boot environment ?

setenv bootargs_base console=ttymxc0,115200

setenv bootargs_mmc 'setenv bootargs ${bootargs_base} root=/dev/mmcblk1p1 rootfstype=ext3 rootwait rw ip=dhcp'

setenv bootcmd_mmc 'run bootargs_mmc;mmc dev 2;mmc read ${loadaddr} 0x800 0x2000;bootm'

Regards,

Weidong

1,170 Views
vishvapathi
Contributor V

Hi Weidong,

After giving udhcpc command eth0 was enabled and now i am able to ping the server.

Thanks for your support

0 Kudos
1,170 Views
weidong_sun
NXP TechSupport
NXP TechSupport

OK, Good Job !

0 Kudos
1,170 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hi,Vishvapathi,

       you forgot to select FEC driver ! :smileyhappy:

weidong

0 Kudos
1,171 Views
vishvapathi
Contributor V

The linux kernel was without ethernet. Activated  by:

  ipconfig eth0 up                    // to load the FEC driver

  udhcpc                                // to obtain the IP address via DHCP when required.

and it works now..

thanks


0 Kudos