Hello, we're using a custom board based on mpc5200b
We are using kernel 2.6.33 and when we using ethernet, we get 80% packet loss with ping.
Where could i find the solution?
U-boot information:
CPU: MPC5200B v2.2, Core v1.4 at 132 MHz
Bus 132 MHz, IPB 132 MHz, PCI 66 MHz
Board: Ran Controller Board
I2C: 85 kHz, ready
Thanks
Lorenzo
Dear Lorenzo
I want to migrate from kernel 2.6.16 to any newer working (kernel 2.6.28 ) one for my
lite 5200b board. pls suggest
---Ramesh
Dear all
I have u-boot latest version with latest kernel (3.5.x)
it is working fine...
Enjoy the Device tree concepts...was introduced...
Power PC with latest kernel power...Ever Green..
Thanks all
--Ramesh
Now i'm thinking that one of main problem is 1:1 cpu:bus ratio, is possible?
Thanks
Lorenzo