problem with usb host

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

problem with usb host

562 Views
alejandro_df
Contributor I

the program sends me error in the read and write command in usb host mode, when I run the example USB_MSD_HOST_MKL25Z128_PEx sends me the following result:

TERMINAL.PNG


I've already tried three different usb stick and sends me the same result.I'm using the usb stack 4.1.1 help me

Tags (5)
0 Kudos
2 Replies

316 Views
santiago_lopez
NXP Employee
NXP Employee

Hi Alejandro,

Are you using a TWR-KL25? or a FRDM_KL25? I´m asking this because the host must provide the 5V on VBUS and the FRDM-KL25 can´t do this natively (hardware modifications are required)

Saludos

0 Kudos

316 Views
diegocolombo
Contributor IV
0 Kudos