AnsweredAssumed Answered

i.MX6Q Sabre Lite USB RECOVERY FAILED

Question asked by Younes CHALABI on Jul 2, 2013
Latest reply on Sep 7, 2013 by nehal omran

Hi all,

 

My board does not boot. I have no display on the output serial line. When trying to flash it via USB OTG, I can't find the Freecale entry via the lsusb command. Here is the log of the dmesg command :

 

younes@younes-Latitude-E6530:~/Younes/Sabre$ dmesg | tail

[ 6796.833407] usb 3-1: device not accepting address 36, error -71

[ 6796.945409] usb 3-1: new full-speed USB device number 37 using xhci_hcd

[ 6796.945537] usb 3-1: Device not responding to set address.

[ 6797.149514] usb 3-1: Device not responding to set address.

[ 6797.353319] usb 3-1: device not accepting address 37, error -71

[ 6797.465344] usb 3-1: new full-speed USB device number 38 using xhci_hcd

[ 6797.465505] usb 3-1: Device not responding to set address.

[ 6797.669454] usb 3-1: Device not responding to set address.

[ 6797.873275] usb 3-1: device not accepting address 38, error -71

[ 6797.873314] hub 3-0:1.0: unable to enumerate USB device on port 1

 

Do somebody has an idea of where it may come ?

 

Thanks

Outcomes