AnsweredAssumed Answered

Changing processor for a CW10.4 project?

Question asked by Frank Van Hooft on Jul 1, 2013
Latest reply on Jul 1, 2013 by ZhangJennie

Apologies for the newbie question. Using CW10.4 under Windows I've imported the project for AN4370 (USB bootloader for the K20) and it's building fine. I need to actually target the KL25 processor. I understand I need to change the linker file. But how do I change the target processor? I see in the project properties it's saying Cortex-M4, but where can I change it to Cortex-M0?  (And is there anything else I should be doing?)

 

Thanks a lot.

Outcomes