an2295 serial boot loader on MCF52259

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

an2295 serial boot loader on MCF52259

457 Views
shenlung
Contributor II

Good day, I download app note sw and has folder for MCF52259, but unable to get working. Board is same as MCF52259 demo. Want to use uart0. I have the codewarrior 10.2 and the classic 7.2. Both versions the import is not clean, There are missing MCF52259_Internal_flash.cfg and MCF52259_Internal_flash.mem

I dont know if that the problem. It seems to compile ok.  I've tried generating new target and launch configurations in 10.2 but getting lost.

 

I know the board works fine because I have an MQX project that runs on it. I want to be able to load up the MQX proj via serial fiber link since bdm port not easily accessible.

 

thx

Labels (1)
0 Kudos
0 Replies